What is the maximum input voltage range of the ATV6XX "N4" Process family drive?
Issue:
Maximum input voltage range of the ATV6XX "N4".

Product Line:
Altivar 6XX process drive family

Environment:
All models, All serial numbers.

Cause:
N/A

Resolution:
The range of the input voltage for the ATV6XX Process drive family is 380 - 15% to 480 +10% or a range of 323 to 528VAC, three phase.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: