Where can I locate the serial number on the ATS48 softstarts?

Article available in these languages: Spansk

Issue:
Needs the serial number of an ATS48

Product line:
ATS48, Altistart 48

Environment:
all

Cause:
n/a

Resolution:
The serial number is printed under the bar code on the nameplate.  The nameplate is located on the right hand side of the ATS48.  See the photo example attached.




Schneider Electric Danmark

Bilag
ATS48 serial number location.bmp [2.16 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: