How do I view Machine Expert HVAC - SoMachine HVAC variables in Vijeo Designer?
Vijeo Designer uses ModbusRTU or Modbus/TCP to read and write data to a M171/172 HVAC controller. Only Machine Expert HVAC - SoMachine HVAC Status Variables have an assigned modbus address. Therefore only Status Variables can be Viewed and written to by a Magelis HMI. You can define Status Variables in you SoMachine HVAC project in the Resources Tab. When you create a Status Variable, Machine Expert HVAC - SoMachine HVAC automatically assigns an address to the variable. Such as 8960. In Vijeo Designer you would reference that address by using 48960 in your variable definition window.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: