Video: How to view measurements, event logs and disturbance records directly from a MiCOM Px40 series relay
Issue
The user would like to view measurements remotely via Easergy Studio ( formerly known as MiCOM S1 Studio) as well as retrieve on-board event logs and disturbance records.

Product Line
Easergy Studio

Resolution
The video below explains how to view any available measurement and download event logs and disturbance records directly from the Micom Px40 relays using Easergy Studio. The user needs to download and install Easergy Studio before proceeding with this video. This video assumes that the relay is pre-configured and can communicate over Ethernet, serial or using the front panel DB-9 port. Attached below is the Easergy Studio Help Guide as a reference.

Schneider Electric Danmark

Bilag
Easergy_Help_Guide.zip [1.45 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: