Can the ATV630 process drive be programmed for anti jam?
Issue:
ATV630 process drive set up for anti jam.

Product Line:
Altivar ATV630 ATV660 process drives

Environment:
All

Cause:
Anti Jam function Programming

Resolution:
Yes, the ATV630's Anti Jam function allows the pump to execute forward, and then reverse pump rotation cycles. See the attached file for programming assistance.

Schneider Electric Danmark

Bilag
Anti Jam function on the ATV630 Process drive.pdf [249.54 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: