How low can the motor thermal current be set on the ATV12 drives when you are running a smaller size motor on the drive?
Issue:
Set motor thermal current on the ATV12 drives when you are running a smaller size motor.

Product Line:
Altivar 12

Environment:
All

Cause:
Wants to know what is the smallest size motor you can put on the ATV12 drive and still have motor thermal protection.

Resolution:
You can program the Nominal drives motor current to 25% of the drives current IN ratings.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: