Unity Pro V11.0: section execution condition of DFB not taken in account.
Goals and Symptoms
On BME P58 5040(C), BME P58 6040(C) and BME H58 6040(C) PLCs, section execution conditions of DFB are not taken in account: sections of DFB are always executed even if the conditions are false.

Causes and Fixes
Install the hot fix UnityPro_V110 HF0339925R to fix the issue on Unity Pro V11.0
Unity Pro V11.1 corrects this misbehavior.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: