Make a backup of ClearSCADA Mobile configuration.
Configuration of ClearSCADA Mobile Server can be backed up by making a copy of the MobileConfig.sdf configuration file located in
  • C:\ProgramData\Schneider Electric\ClearSCADA Mobile (prior to ClearSCADA 2017 R2)
  • C:\ProgramData\Schneider Electric\ClearSCADA (in ClearSCADA 2017 R2 and newer)

The MobileConfig.sdf file contains a list of Mobile Systems, Mobile Devices and Mobile Users. ClearSCADA Mobile Server License is also stored in this file. The configuration file can be found on the machine hosting ClearSCADA Mobile Server.
Note: The current configuration file must be named MobileConfig.sdf. Do not change the name of the MobileConfig.sdf currently in use by the Mobile Server as it will result in loss of configuration.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: