Is there an address to read status of the RJ-45 ports on the Altivar Process Profinet Card?
Issue:
Address to read status of the RJ-45 ports on the Process Profinet Card.

Product Line:
ATV630, Altivar 630, Altivar Process

Environment:
All

Cause:
Customer wants to know if Port A or Port B on the Profinet Card is up or down

Resolution:
With last version of Profinet V1.6, it's not possible to see the  port status with Modbus address or PNU address. The information is not accessible this way. However, you can read status only by LLDP service. See attachment.

Schneider Electric Danmark

Bilag
Profinet_PortStatus.pdf [220.79 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: