Video: How to change the temperature thresholds on a Network Air FM unit
Issue:
This document contains a video on how to change the temperature thresholds on a Network Air FM unit.

Product line:
FM35-50, ACFM, IR40.

Environment:
All Serial Numbers.

Cause:
Install Operation.

Resolution:


How to change the temperature thresholds on a Network Air FM unit follow the below procedures.
1 Press ESC until you reach the main menu (On/Off).

2 Scroll to SETUP and press ENTER.

3 Scroll to SYSTEM 1 and press ENTER.

4 Press ENTER on ALARMS.

5 Press ENTER on TEMPERATURE THRSHLD.

6 Select which threshold you want to change and then press ENTER.

7 Use the UP or DOWN arrows to select the desired temperature.

8 Press ENTER when finished.

9 Press ESC until you get back to the status screen.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: