Where should a dynamic braking resistor be installed on an ATV320?

Article available in these languages: Czech, Græsk, Japansk

Issue:
Wiring a braking resistor in ATV320 drives.

Product line:
ATV320, Altivar 320

Environment:
all

Cause:
Adding braking resistor

Resolution:
The ATV320 has 2 model types.
On the ATV320...B drives, the braking resistor should connect between terminals PB and PBe.
On the ATV320...C drives, the braking resistor should connect between terminals PB and PO.

Also, verify that parameter brA (Deceleration Ramp Adaptation) is set to NO.  Factory default for brA parameter is Yes.  The drive will not use the braking resistor if brA is set to Yes.  The brA parameter can be found at the following menu location:  COnF - FULL - FUn - rPt -rPt- brA.

See the ATV320 Installation Manual for any further details.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: