How do you set up the ATV320 drive so that the digital DO output controls output contactor command OCC?
Issue:
Set up the ATV320 drive so that the digital DO output controls output contactor command OCC.

Product Line:
ATV320

Environment:
All

Cause:
Wants to set up the DQ or DO so that it controls the a output for OCC.

Resolution:

Wiring:
Jumper +24vdc to DQ+
Wire your + side of your relay coil to DQ-
Wire the other side of the coil to Com

Programming:
In the Application Function Menu, set OCC to DO1

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: