What is the syntax / URL / script for opening directly an object from PLC application program accessible via webpage of BMENOC0311
The program viewer information should be enabled in the Unity application under tools > Projects Settings > PLC Diagnostics.
The firmware loaded in BMENOC0311 should be equal or above V2.07

The syntax / URL / Script is as follows
http://{IP_ADDRESS.EN_US}/#monitoring/plcpv?showConsole=0&showTreeview=0&section=Section_Name|Object_Name&standalone=1

Where IP_ADDRESS is the IP address of BMENOC0311.
SECTION_NAME is the name of the section used in the PLC program
OBJECT_NAME is the name of the variable used in the ladder logic program and is the object identifier in case of the FBD program

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: