Which ConneXium DRS switches can be used with M580 Remote I/O offer?
Issue:
I want to implement the M580 with DRS Architecture.
Which ConneXium DRS switches can be used with M580 Remote I/O offer?

Product Line:
M580
Connexium Switch

Environment:
EcoStruxure Control Expert
Internet Explorer

Resolution:
The Dual Ring Switches (DRS) that can be implemented with M580 Remote I/O to extend the performance of the architecture are the following:
  • TCSESM083F23F1 (8TX 1280) : 8 COPPER PORTS
  • TCSESM063F2CU1 (6TX/2FX-MM) : 2 multi-mode fiber ports + 6 copper ports
  • TCSESM063F2CS1 (6TX/2FX-SM) : 2 single-mode fiber ports + 6 copper ports
You can achieve up to 2 km with multi-mode fiber cables and up to 15 km with single-mode fibre cables in a PlantStructure system.
Up to 15 DRS can be implemented in one architecture.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: