Provide band range for Solo wireless pushbutton XB5R*, ZBRR*

Article available in these languages: Fransk

ZigBee has 16 channels from 2405 to 2480 MHz. These frequencies are the center frequencies.
Each channel is separated by 5MHz but the channel bandwidth is 2 MHz
Our product is adjusted on the first channel 2405 MHz (channel 11). See attachment

To avoid any interference and keep a safety gap, the frequency band should be selected outside 2403,75 MHz - 2406,25 MHz

Schneider Electric Danmark

Bilag
Solo Zigbee frequency.png [62.58 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: