Can the sliding doors from HyperPod be used on an EcoAisle?
Issue:
Can EcoAisle doors be used with a HyperPod.

Product Line:
EcoAisle, HyperPod

Environment:
All versions and serial ranges

Cause:
The sliding doors used with HyperPod are very cost-effective.

Resolution:
The first release of the HyperPod, are not compatible with EcoAisle.  HyperPod doors do not adapt to EcoAisle.  There are no plans currently to make them fit.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: