Are NetShelter SV cabinets compliant for seismic installation?
Issue:
The customer would like to know if the NetShelter SV cabinets are rated for seismic installations in UBC High Seismic Area or OSHPD.

Product Line:
NetShelter SV

Environment:
All versions and serial ranges

Cause:
A customer is looking for a seismic rated cabinet.

Resolution:
The NetShelter SV cabinets are not rated for seismic installation. There are no brackets or accessories that can make them compatible for a seismic installation.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: