Is Metasys N2 communication protocol available for the Atlivar Process drives?

Article available in these languages: Spansk

Issue:
Customer is replacing an old ATV61 drive with Metasys N2 card.  Wants to be able to control and communicate to the drive using Metasys N2.

Product line:
Altivar Process, ATV630, ATV930,

Environment:
All

Cause:
Is there a cross refernce that includes Metasys N2

Resolution:
The Process Drives do not have a Metasys N2 Communication card available. Customer will need to use a third-party Modbus RTU to Metasys N2 gateway.
The Altivar 212 for Fan and Pump applications may be an option, as that drive does have integrated protocols including Metasys N2.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: