How can I get a Ramp stop on S-Flex series E?
Issue:
Customer ordered an S-Flex unit that came with Series E wiring.  They want to make the motor stop on a ramp.

Product line:
S-Flex

Environment:
Series E only.

Cause:
Addition of a run permissive ahead of the AFC-BYP selector switch.

Resolution:
Per Marketing and Engineering, the series E S-Flex was designed for coast to stop applications only.  It is up to the customer to modify the wiring to get a ramp stop function if needed.  Consider adding an additional control relay for drive running status and incorporate a contact in parallel with the RPR contact before the AFC-BYP selector switch, using DIN terminals 4 and 7.
See attachment for several possibilities.

Schneider Electric Danmark

Bilag
Ramp stop options Ser E SFlex.pdf [354.62 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: