What are the new features in SoMachine Basic v1.3 SP1?
The new features in SoMachine Basic v1.3 SP1 are:

New controller starting mode: "Unconditional start in Run" (allows controller to start in Run after applying power without battery charged or present)
Memory Consumption View
Trace
Report (Print): cover page, project info, symbol list, cross-ref, user program (IL+LD)
Symbolization of function block members
Possibility to remove temporary project protection

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: