How to get the week number of the year by program in M580 application ?
For M580 PLC, the WEEK_OF_YEAR EF is not available and the system word %SW70 is giving the week of the year in UTC Time format. To get it in Local time you can import the attached DFB the output is giving the week of the year  in the Local Time (defined by the Project Settings->General->Time (Time Zone)).
The value is decimal from 1 to 52.

DFB in attachment

Schneider Electric Danmark

Bilag
week_of_the_year.zip [933 Bytes]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: