Is there a blank NetShelter door badge available? If so, what size is available and how many are in the package? Can APC provide custom door badges?
Issue:
Customers may want to have their logo on the cabinet.

Product Line:
NetShelter SX

Environment:
All models, all serial numbers.

Cause:
Customers may not want the APC by Schneider Electric logo on their cabinets, or may want additional badges.

Resolution:

We offer sku AR7001X384, which is a pack of 40 blank door badges, The door badge is oval, and the dimensions are 71.5 mm wide x 39.4 mm high.
To date we have not offered custom printed door badges attached to the cabinet. To process a request please contact your APC Sales Rep, or the CustomRacks team.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: