Can I display torques as 'Foot Pounds' on the ATV630 / ATV690 series drives?
Issue:
Change unit of torque to "Foot Pounds" on Altivar Process Drives ATV630/930

Product Line:
ATV630, ATV690 series drives.

Environment:
All models with firmware 1.6 or below.

Cause:
Information unavailable in current literature.

Resolution:
Currently, it is not possible to display torque as foot pounds on the ATV630 and ATV930 series drives.  This information is current as of firmware release 1.6.  An evolution has been created to have this feature added via a future firmware update.  There is no ETA for this firmware release.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: