What are the part numbers for SoMachine version 4.3?
Issue:
Customer needs the part numbers for the SoMachine version 4.3 programming software.

Product Line:
PLC
Programming software

Resolution:
The part numbers for SoMachine version 4.3 are:

- SOMNACS43 + trial license for V4.3 (21days) - USB flash drive. The USB flash drive is mandatory and supplied with a trial license.
- SOMNACCZXSPAZZ 1 (Single License)
- SOMNACCZXTPAZZ 10 (Team License)
- SOMNACCZXEPAZZ 100 (Entity License)

Supported controllers:

- Logic controllers: Modicon M238, Modicon M241, Modicon M251, Modicon M258
- Motion controllers: Modicon LMC058, Modicon LMC078
- HMI controllers: Magelis SCU, XBTGC, XBTGT/GK
- Drive controller: Altivar IMC

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: