What are the direct connection voltage limits for PM2225 meter ?
The meter's voltage measurement inputs are rated by the manufacturer for up to
277 V L-N / 480 V L-L. However, the maximum voltage allowed for direct
connection may be lower, depending on the local electrical codes and regulations.

As per installation category II / III the maximum voltage on the meter voltage
measurement inputs should not exceed 277 V L-N / 480 V L-L for CAT III and 347
V L-N / 600 V L-L for CAT II.

If your system voltage is greater than the specified direct connect maximum
voltage, you must use VTs (voltage transformers) to step down the voltages.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: