Why does an Altivar drive HMI display flash or blink during run state?

Article available in these languages: Japansk

Issue:
Altivar Drive HMI blinking during run status.

Product Line:
ATV12  ATV312  ATV32  ATV320

Environment:
All models

Cause:
HMI is flashing

Resolution:
A flashing HMI display indicates that the current limitation is being exceeded.
Verify the drive settings for nCr, nSP, UnS and CLI
Monitor motor current when the drive is running, for overcurrent condition.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: