Whether Withdrawable or Fixed NSX MCCB can be installed in Horizontal Position ?
The Compact NSX circuit breakers may be installed  horizontally, vertically or flat on their back, without derating performance levels.
There are three installation versions:
1. Fixed
2. Plug-in (on a base)
3. With draw-able (on a chassis).
For the Plug-in and Withdrawable versions the components must be added (base,chassis) to the fixed version.

For details pl refer the attachment.

Schneider Electric Danmark

Bilag
Device Installation_NSX Catalog _2016_LVPED208001EN.pdf [468.57 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: