What needs to be done to the ATV320 drive if you are using a ungrounded IT system?

Article available in these languages: Spansk

Issue:
ATV320 needs to use unground IT systems

Product Line:
Altivar Machines, Altivar 320

Environment:
All models and serial numbers

Cause:
IT ungrounded system

Resolution:
See the attached document IT grounding ground screw removal.pdf for the 230V drives, 400/460V B version drives and 400/460V C  version drives 4.0 kW and smaller.
For ATV320U55N4C - ATV320D15N4C see attached document IT_Jumper_ATV320_N4C.pdf

Schneider Electric Danmark

Bilag
IT grounding ground screw disable.pdf [942.97 KB]
IT Jumper_ ATV320_N4C.pdf [315.15 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: