What can cause an INF2 fault on the ATV71 drive?

Issue:
ATV71 drive with INF2 fault.

Product Line:
ATV71

Environment:
All models

Cause:
The Drive trips in INF2 fault when the software version is incompatible with the application and control motor boards.

Resolution:
Check the reference of the power board and its compatibility.  Re-flash the control board or replace it.  Reseat the power card and control card, and try to power cycle the drive.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: