The EasyPact EZCV with earth leakage protection is compatible with reverse feeding?
The EasyPact EZCV with included earth leakage protection can be supplied from the top or bottom (reverse feeding) with the following restriction: the supply voltage must be below 240V AC.
For voltages above 240V AC the EZCV is compatible with supply from the top side. The Line and Load sides are marked on the front cover of the device for guidance.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: