What is the acceptable input voltage range for Altivar 6xx and 9xx Process Drives?
Issue:
Acceptable input voltage range for Altivar Process Drives ATV630/930

Product Line:
Process Drive

Environment:
All

Cause:
Supply Line Voltage

Resolution:

The line voltage tolerance is +10% and -15%.

Per the ATV600 and ATV900 Catalog, the range is as follows:
- 200 - 15%...240 + 10% three-phase for ATV…M3
- 380 - 15%...480 + 10% three-phase for ATV…N4
- 500 - 15%…690 + 10% three-phase for ATV….Y

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: