Is there a maximum number of writes to assign a Flash Memory PCMCIA TSXMFPP0002M?
Issue
Is there a maximum number of writes to assign a Flash Memory PCMCIA TSXMFPP002M?

Product Line
TSX Micro, TSX Premium

Environment
TSXMFPP002M

Resolution
The PCMCIA card TSXMFPP002M has a ST  Flash IC M29W160 and the average value of writes is 100,000 Program/Erase cycles per Block.
P.S.: Attached is the flash memory datasheet.

Schneider Electric Danmark

Bilag
Datahseet.pdf [665.25 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: