Where can I find the information on the maximum input line currents for the ATV320 drives?
Issue:
Maximum Input Line Currents specifications for an ATV320

Product Line:
Altivar ATV320

Environment:
All

Cause:
Designing power circuit

Resolution:
The maximum input line currents are published in the installation manual NVE41289.
https://www.se.com/ww/en/download/document/NVE41289/

All Altivar Drive and Altistart Softstart Manuals
http://www.altivardrives.com/3

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: