Can the NetShelter CX fans be turned on/off, or fan speed raised/lowered, remotely?
Issue:
A customer asks if the Net Shelter CX fans can be controlled remotely.

Product Line:
NetShelter CX

Environment:
All models, all serial numbers.

Cause:
For various reasons the customer may want to reduce fan speed, or turn them on/off.

Resolution:

Using either NetBotz or a Switched Rack PDU you can control a specific port on the NetBotz or PDU. A temperature sensor can also be used to set thresholds for alarms, or to turn outlets on/off. Please contact your APC Representative to design a solution that suits your particular needs.

NetShelter CX fan speed cannot be raised or lowered remotely, but the AR40xxA and AR40xxIA (and all X-options) have a fan booster switch on the rear. This booster switch allows the customer to increase the standard fan speed.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: