Is there any documentation comparing the Sepam relay to the SEL-751 relay?
Issue
A customer would like documentation comparing our Sepam relay to SEL-751.

Product Line
Sepam 20 series
Sepam 40 series

Environment
Documentation

Resolution
Please find two documents attached. One compares the Sepam 42 to the SEL-751 and the other compares the Sepam 24 to the SEL-751A (I).

Schneider Electric Danmark

Bilag
Comparison Guide - Sepam S42 to SEL-751.pdf [134.32 KB]
Comparison Guide - Sepam S24 to SEL-751A-I.pdf [134 KB]