How do I lock out or disable all parameter changes on the ATV212, used with the VW3A1101?

Article available in these languages: Spansk

Issue:
Is there a way to lock out or prevent parameter changes on the ATV212, in the drive or using with the VW3A1101 graphic display?

Product Line:
Altivar 212

Environment:
All models and serial numbers

Cause:
N/A

Resolution:
Press the Mode (ESC on Graphic Display) button until you see AUF [Quick Menu]
Scroll down to F - - - [Extended Menu]
Press Enter and scroll to F700 [Parameter Lock]
Press Enter and 1 = Locked, 0 = Unlocked
d

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: