How to reset a Magelis / Harmony application from too many login attempts with Vijeo Designer V6.2?
Issue
The HMI is locked out after attempting to login with an incorrect password too many times.

Product Line
Vijeo Designer (all versions)

Environment
HMI Configuration Software, Physical HMI

Resolution
The Password Management feature in Vijeo Designer provides the ability to lock out the user after too many failed attempts. If the user ever gets locked out, the application must be redownloaded to the HMI over USB Memory Stick (via the File System Download Method). If the Download security and the USB Media Install was activated in the application, the HMI must be sent in to have the firmware flashed at the repair center via https://www.schneiderelectricrepair.com/

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: