What is the process to update the firmware version of the TCSEGPA23F14F (PRM)?
Issue
The latest firmware version of the PRM is v1.3 and customer wants to update from older versions.

Product Line
PRM (TCSEGPA23F14F)

Environment
TCSEGPA23F14F

Resolution
The TCSEGPA23F14F (PRM) is a standalone module designed to provide Profibus DPV0 & DPV1 master capability to the M340, M580, Premium and Quantum ranges. The steps below show you how to update the firmware of this module:
1. With Windows Explorer, copy the firmware file in the following directory:
- By default (For PRM Master DTM in Windows 32 bit)
C:\Program Files\Schneider Electric\ PRM master DTM\ Firmware\
-Or <Your_installation_directory>\Firmware\
- By default (For PRM Master DTM in Windows 64 bit)
C:\Program Files (x86)\Schneider Electric\ PRM master DTM\ Firmware\
-Or <Your_installation_directory>\Firmware\
- By default (For PRM Gateway DTM in Windows 32 bit)
C:\Program Files\Common Files\Schneider Electric Shared\PRM Gateway DTM\Firmware\
-Or <Your_installation_directory>\Firmware\
- By default (For PRM Gateway DTM in Windows 64 bit)
C:\Program Files (x86)\Common Files\Schneider Electric Shared\PRM Gateway DTM\Firmware\
-Or <Your_installation_directory>\Firmware\
2. Rename it PRMOS.bin
3. In the Menu bar of Unity Pro, select Tools-> DTM Browser.
4. In the DTM Browser, select <->PRM_Master or <->PRM_Gateway instance.
5. Right-click <->PRM_Master or <->PRM_Gateway instance, and then click Connect.
6. Right-click <->PRM_Master or <->PRM_Gateway instance, and then click Device Menu-> Download Firmware.
The new firmware has been downloaded into the PRM and PRM will reboot with the new firmware.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: