ATV320 how to adjust directly the speed reference via the jog dial
Issue:
How can I adjust the speed from the jog dial on the drive?

Product Line:
Altivar ATV  Process Drive

Environment:

ALL

Cause:

Programming Wiring


Resolution:
To do the same as ATV312 after pressing Mode key.

ConF > FULL > CtL >
Fr1 = A1U1
CHCF = SEP (hold 2s)
Cd1 = tEr
ESC back to RDY

You can now press Enter (Dial) 3x to adjust the speed

Schneider Electric Danmark

Bilag
Command terminal HM 3.docx [40.84 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: