How to connect to the Masterpact MTZ via Bluetooth [Video]

Article available in these languages: Spansk, Tyrkisk

Question:
How to connect to the Masterpact MTZ via Bluetooth

Product String Reference:
  1. Top Level > Product Category > Buildings & IT > Partner Project Transactional > Air Circuit Breakers > ACB MTZ Communication
  2. Top Level > PR_Product_OPS_Structure > Circuit Breakers and Switches > High Current Air Circuit Breakers > Masterpact MTZ

Objective:
The objective of this video is to provide guidance of how to communicate with a Masterpact MTZ via Bluetooth



Product Line:
High Current Air Circuit Breakers

Environment:
N/A

Resolution:
  1. Download the Masterpact MTZ from the Play Store or App Store. Register if required.
  2. The Bluetooth will work once the Micrologic X is supplied with power. Activate the Bluetooth from the Micrologic X.
  3. Click Bluetooth from the App and Discover Device
  4. Click the device from the App. It will ask for a connection request
  5. Enter the pin from the Micrologic X and you will be taken to the device from on your phone
  6. From this app, you can see the following status’ for your MTZ
    1. Health state,
    2. Last trips,
    3. Current per phase

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: