Is there a function block in SoMachine V4.3 to extract the bits of a words?
Issue:
Looking for a way to extract or set a bit within a word.

Product Line:
SoMachine, EcoStruxure Machine Expert

Resolution:
Sometimes it becomes necessary to extract or set a bit within a word.

Those function blocks can be found under the Functionblocks section under Bit/Bytes Functions of SoMachine V4.3.  Or you can simply type in WORD_AS_BIT or BIT_AS_WORD on the empty box.

The block also have to have a unique instance name.



Schneider Electric Danmark

Bilag
W2B_FB.jpg [120.54 KB]
W2B.jpg [36.25 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: