Video : How to configure the Advanced Generic EDS DTM to the BEMNOS0300?
Issue
How to configure the Advanced Generic EDS DTM to the BMENOS0300?

Product Line
Modicon M580, BMENOS0300, EcoStruxure Control Expert (formerly Unity Pro)

Environment
Unity Pro v12, BMENOS0300,  BMEP581020 v2.50

Resolution
The BMENOS0300 has a 16 Byte DDT, which you can interrogate to diagnose the status of the module and this is shown on this video.


Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: