Where can I find information on migrating from an ATV312 to an ATV320?

Article available in these languages: Spansk

Issue:
Transfer files from an ATV312 to an ATV320?

Product Line:
Altivar 312, Altivar 320

Environment:
All

Cause:
Migrating from ATV312 to ATV320

Resolution:
You can find the ATV312 to ATV320 Migration Manual here:
https://www.se.com/ww/en/download/document/QGH39563/

The manual is also attached.

Schneider Electric Danmark

Bilag
schneider-vfd-atv312-to-atv320-migration-manual.pdf [1.17 MB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: