Can the IO module be used for ground fault alarm?
Issue:
Can the IO module be used for ground fault alarm with Masterpact and Powerpact breakers?

Product Line:
Circuit Breakers

Environment:
Powerpact P and R, Masterpact NT and NW.  With P and H trip units.

Resolution:
Yes. EcoStruxure Power Commission software version 2.12 released March 29, 2019  has GF alarm functionality through FW update to the IO module. EcoStruxure Power Commission software prior to version 2.12 does not have GF alarm functionality.

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: