What is an internal serial link fault (INF3) on an ATV320 drive?
Issue:
Internal serial link fault (INF3) meaning on an ATV320.

Product Line:
Altivar 320

Environment:
All

Cause:
Communication interruption between internal cards of VFD

Resolution:
Check internal connections.
If there is an option card, remove and re install.
Power cycle the VFD.
Factory reset if needed.
Power up with no option card if installed (this will perform factory reset)

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: