Does XBTL1000 support Windows 10?
Issue:
Inquiry regarding if XBTL1000 supports more modern operating Systems. Support for Windows XP from Microsoft has ended and support for Windows 7 will end soon. Looking to see if XBTL1000 can run on Windows 10.

Product Line:
XBTL1000

Resolution:
No, XBTL1000 does not support Windows 10. It is suggested to use a Virtual Machine running Windows XP or Windows 7 if you only have a Windows 10 PC.

Schneider Electric Danmark

Se mere
Produkt:
Artikler som kan være nyttige
Se mere
Produkt: