Søg i ofte stillede spørgsmål
What is the latest firmware for the BMXNOM0200 module?
Issue
Customer needs to verify the current BMXNOM0200 firmware revision.
Product Line
M580, M340, X80
Resolution
As of June 14th, 2023 v1.6 is the latest firmware available.
Customer needs to verify the current BMXNOM0200 firmware revision.
Product Line
M580, M340, X80
Resolution
As of June 14th, 2023 v1.6 is the latest firmware available.
Udgivet til:Schneider Electric Danmark
Bilag
Se mere
Produkt:
Område:
Se mere
Produkt:
Område: