How to coordinate the start address of IOscanner at BMENOC0301 of M580 system to communicate with Quantum
Question:
How to coordinate the start address of IOscanner at BMENOC0301 of M580 system to communicate with Quantum?

Answer:
Inside IO scan configurator of M580 system, the RD Address/WR Address is referring to address of counterpart.
Since M580 starts from %MW0 while Quantum start from %MW1, you have to assign the address 99 at  M580 IOscan configurator to correspond to the address 100 at Quantum.

Schneider Electric Danmark

Bilag
IOscan.png [331.49 KB]
Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: