How do I perform a Factory Reset of an ATV340 drive via the keypad?
Issue:
Customer wants to reset the programming to factory default using the keypad of the drive.

Product Line:
ATV340 series

Environment:
All

Cause:
NA

Resolution:

Go to Menu 7: Files Management and press enter. Scroll down to 7.2: Factory Settings and press enter.

Scroll down to Parameter group list and press enter, select "All" if a full factory reset is needed. Press ESC to go back.

Scroll down to Go To Factory Settings and press enter. A Warning message will appear, press ENT again to continue.

Factory reset is done.



NOTE:  It is Always advised to save the current configuration, prior to doing a full factory reset.

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: