Looking for a fixed power factor correction capacitor or PFCD capacitor replacement
Issue
Looking for fixed power factor correction capacitor or fixed PFCD capacitor replacement

Product Line
Fixed PFCD capacitors

Environment
Product selection

Resolution
Schneider Electric no longer has a product offer for fixed power factor correction capacitors in North America.

The latest power factor correction offer is VarSet. VarSet is an automatic capacitor bank, which means that it adapts the quantity of reactive power provided to the system as necessary to achieve the target power factor. VarSet Standard starts at 75 kVAr for 480 V systems and 50 kVAr for 600 V systems. VarSet Detuned starts at 75 kVAr for 480 V and 600 V systems. The minimum step size is 12.5 kVAr or 25 kVAr, depending on the VarSet model.

For more information, including product specifications and part numbers, please refer to the VarSet - Low voltage capacitor banks - 2022 NAM Catalogue here: https://www.se.com/ca/en/download/document/PFCED310004NAM/

Schneider Electric Danmark

Se mere
Område:
Artikler som kan være nyttige
Se mere
Område: